usr/lib/libc.so: file not recognized: file format not recognized
Hello, I am working with the STM32MP257F-EV1 Development board and I am getting stuck. I am following the following guide: https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP2_boards/STM32MP257x-EV1/Develop_on_Arm%C2%AE_Cortex%C2%AE-A35/Modify,_rebuild_and_reload_the_Linux%C2%AE_kernel. I am doing the step make ${IMAGE_KERNEL} vmlinux dtbs LOADADDR=0xC2000040 O="${OUTPUT_BUILD_DIR}" and when I run make I get the following output:
make[1]: Entering directory '/home/carson.kirk@internal.etherform.com/STM32MPU_Workspace/STM32MPU-Ecosystem-v5.1.0/Developer-Package/stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/aarch64-ostl-linux/linux-stm32mp-6.1.82-stm32mp-r2-r0/build'
GEN Makefile
HOSTLD scripts/dtc/dtc
/home/carson.kirk@internal.etherform.com/STM32MPU_Workspace/STM32MPU-Ecosystem-v5.1.0/Developer-Package/SDK/sysroots/x86_64-ostl_sdk-linux/usr/lib/gcc/x86_64-ostl_sdk-linux/12.3.0/../../../../lib/libc.so: file not recognized: file format not recognized
collect2: error: ld returned 1 exit status
make[2]: *** [/home/carson.kirk@internal.etherform.com/STM32MPU_Workspace/STM32MPU-Ecosystem-v5.1.0/Developer-Package/stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/aarch64-ostl-linux/linux-stm32mp-6.1.82-stm32mp-r2-r0/linux-6.1.82/scripts/Makefile.host:120: scripts/dtc/dtc] Error 1
make[1]: *** [/home/carson.kirk@internal.etherform.com/STM32MPU_Workspace/STM32MPU-Ecosystem-v5.1.0/Developer-Package/stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/aarch64-ostl-linux/linux-stm32mp-6.1.82-stm32mp-r2-r0/linux-6.1.82/Makefile:1524: scripts_dtc] Error 2
make[1]: Leaving directory '/home/carson.kirk@internal.etherform.com/STM32MPU_Workspace/STM32MPU-Ecosystem-v5.1.0/Developer-Package/stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/aarch64-ostl-linux/linux-stm32mp-6.1.82-stm32mp-r2-r0/build'
make: *** [Makefile:238: __sub-make] Error 2
I am unsure how to fix this error. Any help would be greatly appreciated. Thanks!
Carson