Question
Compiling an OLED Display with SSD1306 and Fonts in VS Code
I am testing a very simple OLED display using the SSD1306 driver and fonts, referring to the link below. However, the code does not compile successfully.
Are there any possible reasons for this issue?

/* USER CODE BEGIN Includes */
#include "fonts.h"
#include "ssd1306.h"
/* USER CODE END Includes */
/* USER CODE BEGIN 2 */
SSD1306_Init();
SSD1306_GotoXY (0,0);
SSD1306_Puts ("MICROPETA", &Font_11x18, 1);
SSD1306_GotoXY (0, 30);
SSD1306_Puts ("BY NIZAR", &Font_11x18, 1);
SSD1306_UpdateScreen();
HAL_Delay (1000);
SSD1306_ScrollRight(0,7);
HAL_Delay(3000);
SSD1306_ScrollLeft(0,7);
HAL_Delay(3000);
SSD1306_Stopscroll();
SSD1306_Clear();
int num=2024;
char snum[5];
SSD1306_GotoXY (30,20);
itoa(num, snum, 10);
SSD1306_Puts (snum, &Font_16x26, 1);
SSD1306_UpdateScreen();
//SSD1306_DrawLine(POINT1 X, POINT1 Y, POINT2 X, POINT2 Y, 1);
SSD1306_DrawLine(1,54,126,54,1);
SSD1306_UpdateScreen();
HAL_Delay (5000);
SSD1306_Clear();
// For Rectangle, we need to use two corner points
// SSD1306_DrawRectangle(POINT1 X, POINT1 Y, POINT2 X, POINT2 Y, 1);
SSD1306_DrawRectangle(17,1,115,14,1);
// SSD1306_DrawTriangle(POINT1X, POINT1Y, POINT2X, POINT2Y, POINT3X, POINT3Y, 1);
SSD1306_DrawTriangle(73,22,124,62,74,54,1);
// SSD1306_DrawCircle(CENTER POINT X, CENTER POINT Y, RADIUS, 1);
SSD1306_DrawCircle(34,50,13,1);
SSD1306_UpdateScreen();
/* USER CODE END 2 */