Question
How to implement the function of downloading only the compiled firmware in VSCode?
How can I use VS Code to download only the firmware? I can do it using debug mode, but I don't want to trigger debug. Is it possible to run it automatically after downloading, like CubePRG? I'm not very familiar with CMake. Thank you.
-----------------------------------------------------------------
Erasing internal memory sectors [0 6]
Download in Progress:
2
File download complete
Time elapsed during download operation: 00:00:06.418
-------------------------------------------------------------------
Just take out this part separately