I can't see .cyh files in Visual Studio Code but I can in STMCUBEIDE
Hello community, I have recently used an open source project with STM32 LoRaWAN but I have a certain doubt when opening the project in the STM32CUBEIDE environment I can see the corresponding files, make modifications, compile and run correctly but they appear in the following way with a kind of link icon:

But when I open the same project for reasons of my own convenience in Visual Studio Code, these files do not appear, nor do they appear in my file search engine, I have not been working in this STM32 environment for a long time:

I would appreciate any information and solution on how I could view and edit them in Visual Studio Code, since also if I try to do a git add the files do not appear either, I am attentive, thank you very much.