Issue compiling a project in VSCode: can't find main.h
Hi everyone,
I’m still having an issue with my STM32F746G-Discovery board. I want to run the program using VSCode, but I’m encountering errors in my main.c file. Specifically, it can't find main.h, and as a result, the code isn’t running.
I want to build and run the code directly in VSCode, but it’s not working as expected. Could it be that the compiler is misconfigured? I’m currently using the GCC compiler for C/C++.
I also switched the toolchain in CubeMX to Makefile. After that, I installed CubeCLT and tried to run and build the code, but nothing happened.