[Linux] STM32Cube for VS Code: /dev/ttyACM0 + Debugging issues fixed with STSW-LINK007 + libusb-1.0
Context
Fresh Ubuntu 24.04, STM32 board (ST-LINK/V2-1 0483:374b), STM32Cube for VS Code 3.6.4.
Out of the box, both Serial Monitor and debugging failed:
**** Failed to open the serial port /dev/ttyACM0 ****
Adding myself to dialout didn’t help; debugging couldn’t connect to any target.
Root cause
STM32Cube for VS Code doesn’t install udev rules or USB deps for ST-LINK on Linux. Result:
/dev/ttyACM* gets recreated with restrictive perms on each replug.
The debug adapter (ST custom DAP / libusb backend) can’t init properly.
Fix (repeatable)
Install USB dependency + ST udev rules
sudo apt update sudo apt install libusb-1.0
Download STSW-LINK007, then follow itsreadme.txt.
Replug the board and verify:
ls -l /dev/ttyACM* # example: # crw-rw----+ 1 root dialout 166, 0 Nov 4 16:39 /dev/ttyACM0
Verify debugging in VS Code
Run: Run & Debug → STM32Cube: ST-LINK GDB Server.
Debug now starts normally with ST-LINK/V2-1 and Cube 3.x.