N6 VS Code launch.json for debugging
I'm having some difficulty getting debugging working in VSCode for the N6 series. Does anyone have a sample one that actually works? I'm obviously using the `stlink` server backend for `cortex-debug`, and I have tried using CubeIDE to get the exact gdb-server arguments used when it launches a debug session. However even when I do that, I still end up with a corrupted stack pointer or missing sources? The symptom is that the debug session says something to the effect of "??@<hex> Unknown Source". It also seems to have problems halting the core at startup.
Here's something representative of the config I'm using right now:
{
"version": "0.2.0",
"configurations": [
{
"cwd": "${workspaceFolder}",
"executable": "${workspaceFolder}/FSBL/build/<my_project_name>.elf",
"name": "Debug with ST-Link",
"request": "launch",
"type": "cortex-debug",
"runToEntryPoint": "main",
"showDevDebugOutput": "none",
"servertype": "stlink",
"serverArgs": [
"-l", "1", "-s", "-m", "1", "-k",
],
},
]
}
I've tried using a lot more arguments spelling out all the possible source locations, post-launch commands, etc, but so far it's been to no avail. Any help is appreciated!