Skip to main content
Visitor II
October 28, 2025
Question

STM32CubeIde for VSCode - workspace dirty by ST files all the time

  • October 28, 2025
  • 2 replies
  • 245 views

Hello, 

Long time lurker here. 

First of all, thank you for the extensions, really appreciated the possibility to work directly in vscode.

I have a couple of situation, however, that are really annoying and that I would like to solve.

 

While developing in vscode with the extension enabled. It is sufficient to update the CMake presets in order to have the tools installed by the ST extension to make the git repository dirty.

If before committing the files to the repo a pre-commit that formats the files in a proper way then it is amplificated.

The files:

  •  c_cpp_properties.json in the .vscode folder is always updated with the compileCommands updated if dynamic folders for Debug and Release are used
  •  .clangd configuration file is updated in the CompilationDatabase field.

In my opinion there are two different types of settings:

  •  settings that needs to be persinstent, and maybe reusable on different computers by different users
  • settings related only to the current run

There should exist a good way for switching branches and change configuration without having to worry about the extension that changes files at his willing.

Is it unclear if I can put under gitignore the content of .settings folder. Anyway I cannot place under gitignore the other two files mentioned above because I am using them for other configurations.

 

Thank you in advance

 

    This topic has been closed for replies.

    2 replies

    Graduate II
    October 30, 2025

    @andyi 
    No clue myself about .vscode & .clangd updates and way to kept them static.

    About .settings according to me yes it has to be part of your source controlled assets. Content is part of your project, the first being bundles* files which are the one keeping memory of tools you're using. These files are th way for you to get reproducible results overtime.

    andyiAuthor
    Visitor II
    October 30, 2025

    Thank you for your reply.

    Yes, I can understand about the .settings folder. This is a common topic also with other tools / solutions.

    I do not understand, the .vscode and the .clangd updates. Those are the more annoying.

    My understanding is that the tools are copied and rebranded probably with some customization. It looks to me a bug that those files are updated in this way. No idea about how to notify them as bugs if not writing here...

     

     

    ST Employee
    October 30, 2025

    @andyi 
    Thanks for reporting. I confirm that the ST community is the right place to reach the R&D team.
    I also confirm @Cartu38 OpenDev's OpenDev contribution regarding .settings. As you noticed, this is quite a common practice. No automation is possible without a couple of proprietary metadata files.
    Regarding c_cpp_properties.json and .clangd, internal tickets have been submitted. We will keep you updated here.

    andyiAuthor
    Visitor II
    October 30, 2025

    Thank you for the update.

    Would love to see it fixed. 

    Have a nice day.

    Andrea