VS Code (STM32 Extension) blocks MCU-Finder from starting (Mac OS M1)
Just installed the STM32 Extension to VS Code. If I start the MCU-Finder from within the extension, the MCU banner appears and then hangs in that state. If I quit VS Code while the MCU Finder banner is visible, the MCU Finder will then continue loading and then open.
The MCU Selector also hangs within STM32CubeMX. If I quit VS Code, the MCU selector will open.
Any ideas?
I have STM32CubeCLT, STM32CubeMX (6.9.1) , and STMCUFinder (6.0.0) installed. Mac OS 12.6.8 (M1).
Thanks