Skip to main content
Associate
November 21, 2025
Solved

Build Errors When Using ThreadX with TouchGFX on STM32F746G-DISCO

  • November 21, 2025
  • 1 reply
  • 334 views

Hi ST Team,

I am working on the STM32F746G-DISCO board.

I have ported ThreadX with TouchGFX to this board, and I want to use the ThreadX + TouchGFX sources generated by STM32CubeIDE.

However, I am facing build errors during compilation.
Please find the attached photos/screenshots of the errors.

I request your support in resolving this issue.If possible, please share any relevant documentation, guides, or reference links that explain how to properly integrate ThreadX with TouchGFX on this board.

Thank you,

Best answer by Mahmoud Ben Romdhane

Hello @Abhishekvh76 ,

 

- You need to install TouchGFX 4.26.0 Designer Software.

- Under X-CUBE-TOUCHGFX, Driver, you select Real-Time Operating System: ThreadX.

- You need to be sure that the folder location path does not include a space.

MahmoudBenRomdhane_0-1764065691132.png

- Open ApplicationTemplate.touchgfx.part under TouchGFX Folder through TouchGFX 4.26.0 Designer    Software, generate the code and Run Simulator.

- Import the project through STM32Cubeide

- The build will be finished successfully.

You find in attachment the STM32CubeIDE Project with ThreadX and TouchGFX enabled.

I will be waiting for your feedback.

 

Best Regards.

Mahmoud

 

 

 

 

 

 

1 reply

Technical Moderator
November 21, 2025

Hello @Abhishekvh76 

 

Let me thank you for posting and welcome to the ST Community.

Your request is under investigation, and I will get back to you ASAP.

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
November 22, 2025

Hi ST Team,

I am following up on my earlier query regarding the build errors I am facing when using ThreadX with TouchGFX on the STM32F746G-DISCO board.

Could you please check if there is any update or solution available for this issue?
The build errors continue to appear, and I would like to understand why these errors are being generated.

I am currently using STM32CubeIDE version 1.17.0.
It would be helpful if you could cross-check whether you are also able to reproduce the same errors on your side using this IDE version.

Please let me know if you need any additional logs or project files from my side.

Thank you,
Abhishek

Technical Moderator
November 25, 2025

Hello @Abhishekvh76 ,

For more investigation, could you please provide your Ioc.File.

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.