Can't configure Serial Audio Interface (ioc) with STM32CubeIDE 1.18.0
Hi,
With the latest STM32CubeIDE 1.18.0 (I tried on Mac and Windows), on a brand new project for a STM32H7B0VBT6 mcu. In the ioc, if I try to enable the SAI1 (or SAI2) it let me choose the mode for both SAI A and SAI B but the configuration panel is empty, it also shows a spinning icon when clicking on SAI1 again. I attached a screenshot for reference. Everything else seems fine (I2S, I2C, SPI, ADC, etc).
Any help is welcome! Thank you!