Cannot create “Application-only” project for NUCLEO-H7S3L8 in STM32CubeIDE
Hi all,
Whenever I try to create a new project for the NUCLEO-H7S3L8 board with the Project Structure set to Application only, I get the following error.

I’ve already refreshed updates via Help → STM32Cube Updates and confirmed that my firmware repository contains the latest STM32CubeH7RS package.
The project creation works only if I select Boot along with Application in the project structure. A standalone Application configuration always fails.
Has anyone else encountered this? Is there a workaround to create an Application-only project for this board?