Cant import a project into a workspace
STM32CubeIDE 1.17.0, Win 11 x64
I have a number of related projects in the space workspace (WS). I can copy & paste them into the same WS with no problem within CubeIDE. New project folders are created within the WS directory & show up in the Project Manager list. All these project folders exist within the WS directory.
When I import a project from outside the WS using Open Projects from File System... they import fine & show up in the Project Manager list.
BUT when I try to cut & paste a project folder from outside of the WS directory into the WS directory via Windows Explorer & then try an add it to the Project Manager list in CubeIDE via Open Projects from File System... I get nothing, no import error messages, nothing. The project file doesn't appear in the Project Manager list, nothing!
Anyone know why this is?