Hello @chriskuku
The error you're encountering in STM32CubeIDE—"init mode failed (unable to connect to the target)" and "Operation timed out" indicates that OpenOCD cannot communicate with your STM32 device. This is often caused by hardware connection issues (such as loose or incorrect SWD/JTAG wiring, insufficient power, or incorrect BOOT pin settings), outdated ST-Link firmware, the MCU being in a low-power or locked state, or conflicting software accessing the ST-Link. To resolve this, ensure all hardware connections are secure, update your ST-Link firmware, check that the target board is powered and in the correct boot mode, and close any other software that might be using the debugger. Also, try changing the reset mode in your debug configuration and, if necessary, perform a full chip erase using STM32CubeProgrammer. If the problem persists, test with a different USB port and cable.
THX
Ghofrane