Could not verify ST device on STM32F407VGT6
I have already updated my CubeIDE to the latest version 1.19.0 available on the official website. After writing the code with it, I attempted to download it to my F407VGT6 via STLink, but the download has never been successful. It always prompts "Could not verify ST device!" When I replaced one board with another, I was able to successfully download. The only difference between the two boards is that the silk-screening of the two VGT6s is slightly different. One has a small circle with "e3" inside and can be downloaded, while the one that cannot be downloaded has "e4" in the circle. I wonder if CubeIDE has not yet adapted to this chip. Has anyone encountered the same situation? I hope to get your solution!