Cube Ecosystem - A Rant
For years, ST seems to spit in the face of developers every time they try to “improve” the ecosystem. Even now they’re trying to move toward *** like AI chips or other *** that sounds great to shareholders, while we developers are left with the crumbs of their work. These chips are widely recognized around the world and probably have some of the best engineers in the industry behind them, and yet what we actually get as developers are slow programs programs with a thousand issues on Linux, badly developed no matter how you look at it.
Recently, as Linux programmers, we ran into the problem that CubeProgrammer was using an “hack” I can’t call it anything else where it used an sprintf() on stdin to try to catch all files starting with 0x*. And as soon as this recursive hack stopped working, they blamed Linux for the issue (obviously). All these applications are written in Java and are ridiculously slow, to say the least. An Eclipse-based IDE in 2025 feels like a slap in the face to anyone who wants to produce good software but is dragged down by terrible support that the developers don’t really provide.
Let’s talk about the big problem: CubeIDE. This is supposedly the only “clean” way to work on projects, and it’s the real pachyderm of embedded development. On top of the constant workspace breakages across all platforms, this IDE is nearly unusable. The pseudo LSP barely works, errors are not runtime, there’s no flychecking, and we’re stuck using ***py build systems that aren’t even modern. And honestly, as a developer, I don’t even want a “better Eclipse.” I just want to stop using it. The debugging works well no complaints there but there are simply no real alternative ways to work decently with these poorly maintained products.
HAL often has problems too, and we developers end up touching CMSIS which I guess is the standard for Cortex-M but we’ve truly reached the limit. The development environments need real improvement. And the one they made for VSCode is not an alternative. Maybe ten people use it. And if ST’s developers actually used it themselves, they wouldn’t ignore the fact that it’s full of bugs, integrates poorly, doesn’t genuinely meet developers’ needs, and whenever you start a project you usually have to manually hack together debug integrations because the official one is half baked. At that point you might as well use OpenOCD, which is more stable. BUT everything becomes unstable again the moment you open CubeMX to regenerate the project.
On top of this, CubeMX can generate CMake and Makefiles, which is basically the only sane way to write software in 2025. Most editors need the generation of a CMakeLists.txt, and ignoring this is genuinely *** and counterproductive to the company’s own interests. And since I do everything in nvim and VSCode, it seemed like the only escape from that horrible “IDE” nightmare.
The fact that the CMake option is semi hidden, that ST doesn’t advertise it, and doesn’t even integrate it into the IDE infuriates me, because ST is clearly trying to lock developers into the IDE and avoid giving any way for anonymous project data not to be collected. Then CubeMX doesn’t generate any clean way to compile, flash, or debug. It basically dumps the HAL files with the configuration you asked for and says, “okay, now you handle everything else.” And using comment markers inside files as generation points in 2025 is comica but that’s a rant for another day.
I hate how ST occasionally throws us a “little treat” to keep us quiet, and as a developer this is painfully obvious. I hate how “enterprise” the choice of including an ST microcontroller in your project has become. Because choosing a microcontroller is a choice, and it shouldn’t force you to change your entire toolchain just to accommodate a microprocessor manufacturer even if, being Italian, we’re practically forced to use this giant’s chips.
So I ask ST: do you really want to keep going in this direction? Can’t you create generic tools that let every developer work the way they want, in the best possible way, with the stability that a giant should guarantee? Don’t you want to allow external debugging, or the ability to write real, functional configurations or plugins? Don’t you want to contribute even a little to open source, letting developers expand your ecosystem and make it amazing?
Because what you’ve done or what you did once was great, but we can’t keep praising what was built in the past, especially when the ship we’re sailing on is full of holes. Especially when fixing that ship requires just the minimal effort of not being so greedy, and when all you really need to do is throw out that pachyderm of an IDE and build a clean, universal toolchain without excessive telemetry, without bloatware, extensible, fair for everyone, possibly open, and worthy of the best developers embedded has.
And this isn’t about closing doors I want to open every door possible. I want ST’s developers to cooperate and respond to all these questions. I want consumers (us) to participate and express our opinions with the guarantee of remaining partners of this company (ST) and continuing to build amazing things but starting to do it without constantly smashing our heads against the wall.
I believe we can do it, and I hope that everything I’ve expressed won’t be deleted just to protect the company’s image, but instead can start a conversation that actually improves my life as a developer and the lives of many others.