Cube IDE poor reliability when debugging
Here are some threads which describe the problems
Basically, if you want to do Statistical Profiling, you have to enable PC Sampling and then Cube leaks memory at around 100kbytes/sec. Eventually it crashes, obviously. The SWV ITM debug mode does not need PC Sampling and is thus a lot more reliable, but only in the OpenOCD debugger mode.
Instead of adding more stuff which nobody uses, ST should fix this program properly, starting with the famous "random file opening" issue which about 100 people have complained about.
Another way to crash Cube is to use a STLINK debugger with some unspecified fault on the USB side. Cube just leaks lots of memory and bombs. Poor error detection...