CubeIDE 1.16.1 arm-none-eabi-gdb-version Error
I am using CubeIDE version 1.16.1 to program and flash a STM32F433 MCU.
I am using a SEGGER J-Link flasher.
When I try to run the application I get the following error:
I have tried to manually set the workspace toolchain to local in the toolchain manager.
When I open the toolchain manager, I get an error that it has failed to fetch the toolchain list, in addition to four repositories that it cannot read:
Ignoring the message and setting the local toolchain as it follows


I get the same error when running the code on the MCU:
What should I try to do to fix the error?