Skip to main content
Mohammad A
Senior
February 20, 2020
Question

CubeMX generated STM32 LL GPIO driver problem

  • February 20, 2020
  • 3 replies
  • 1054 views

This is what CubeMX has generated for STM32F103VE mcu for LL GPIO driver:

#define LL_GPIO_PIN_0 ((GPIO_BSRR_BS0 << GPIO_PIN_MASK_POS) | 0x00000001U) /*!< Select pin 0 */
#define LL_GPIO_PIN_1 ((GPIO_BSRR_BS1 << GPIO_PIN_MASK_POS) | 0x00000002U) /*!< Select pin 1 */
#define LL_GPIO_PIN_2 ((GPIO_BSRR_BS2 << GPIO_PIN_MASK_POS) | 0x00000004U) /*!< Select pin 2 */
#define LL_GPIO_PIN_3 ((GPIO_BSRR_BS3 << GPIO_PIN_MASK_POS) | 0x00000008U) /*!< Select pin 3 */
#define LL_GPIO_PIN_4 ((GPIO_BSRR_BS4 << GPIO_PIN_MASK_POS) | 0x00000010U) /*!< Select pin 4 */
#define LL_GPIO_PIN_5 ((GPIO_BSRR_BS5 << GPIO_PIN_MASK_POS) | 0x00000020U) /*!< Select pin 5 */
#define LL_GPIO_PIN_6 ((GPIO_BSRR_BS6 << GPIO_PIN_MASK_POS) | 0x00000040U) /*!< Select pin 6 */
#define LL_GPIO_PIN_7 ((GPIO_BSRR_BS7 << GPIO_PIN_MASK_POS) | 0x00000080U) /*!< Select pin 7 */
#define LL_GPIO_PIN_8 ((GPIO_BSRR_BS8 << GPIO_PIN_MASK_POS) | 0x04000001U) /*!< Select pin 8 */
#define LL_GPIO_PIN_9 ((GPIO_BSRR_BS9 << GPIO_PIN_MASK_POS) | 0x04000002U) /*!< Select pin 9 */
#define LL_GPIO_PIN_10 ((GPIO_BSRR_BS10 << GPIO_PIN_MASK_POS) | 0x04000004U) /*!< Select pin 10 */
#define LL_GPIO_PIN_11 ((GPIO_BSRR_BS11 << GPIO_PIN_MASK_POS) | 0x04000008U) /*!< Select pin 11 */
#define LL_GPIO_PIN_12 ((GPIO_BSRR_BS12 << GPIO_PIN_MASK_POS) | 0x04000010U) /*!< Select pin 12 */
#define LL_GPIO_PIN_13 ((GPIO_BSRR_BS13 << GPIO_PIN_MASK_POS) | 0x04000020U) /*!< Select pin 13 */
#define LL_GPIO_PIN_14 ((GPIO_BSRR_BS14 << GPIO_PIN_MASK_POS) | 0x04000040U) /*!< Select pin 14 */
#define LL_GPIO_PIN_15 ((GPIO_BSRR_BS15 << GPIO_PIN_MASK_POS) | 0x04000080U) /*!< Select pin 15 */
#define LL_GPIO_PIN_ALL (LL_GPIO_PIN_0 | LL_GPIO_PIN_1 | LL_GPIO_PIN_2 | \
 LL_GPIO_PIN_3 | LL_GPIO_PIN_4 | LL_GPIO_PIN_5 | \
 LL_GPIO_PIN_6 | LL_GPIO_PIN_7 | LL_GPIO_PIN_8 | \
 LL_GPIO_PIN_9 | LL_GPIO_PIN_10 | LL_GPIO_PIN_11 | \
 LL_GPIO_PIN_12 | LL_GPIO_PIN_13 | LL_GPIO_PIN_14 | \
 LL_GPIO_PIN_15) /*!< Select all pins */

When I compile it in CubeIDE I get this warning:

large integer implicitly truncated to unsigned type [-Woverflow]

I am using latest version of libraries and CubeMX and CubeIDE.

I had also some problems using pins with number 8 and bigger to control GPIO.

Re-generation of code didn't solve the problem.

3 replies

FAndr.5
Associate II
November 3, 2022

I have same problem, any solution?

Visitor II
April 15, 2025

Same problem in 2025. STMCubeMX Version 6.14.1.

Technical Moderator
April 15, 2025

Hello @edsontomioka ,

 

First let me thank you for posting and welcome to the ST Community.

For more investigation, I suggest please that you provide your Ioc.File.

 

Thanks.

Mahmoud

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Visitor II
April 15, 2025

Sorry, the LLdriver is working fine. My fault.
I used _Pin for direct BSRR register access, but the LL driver _Pin definition is 32 bit unlike HAL driver 16 bit.