Skip to main content
Associate II
September 9, 2024
Solved

Debugging Issues STM32F429I

  • September 9, 2024
  • 2 replies
  • 2996 views

Muthamizh_0-1725860329559.png

 

I HAVE USED THE ST LOADER  YOU HAVE SUGGESTED FOR MY LAST PROBLEM AND NOW ALSO IT REPEATES TEH SAME PROBLEM THERE IS PROBLEM WHILE OPENING THE STM32_PROGRAMMER_CLI.EXE. SUGGEST ME A SOLUTION FOR THIS OR AN ALTERNATIVE.

 

Muthamizh_1-1725860589082.png

THIS IS THE DEBUGGER CONFIGURATION AND THE STLOADER I HAVE SELECTED.

Best answer by mƎALLEm

@Muthamizh wrote:

 i don't find any stldr file for my stm32f429i series.


How? any loader? already provided you one.

Also in the CubeProgrammer, this is the list of all loader available for this board. And the one in the red rectangle corresponds to the NOR Flash loader.

SofLit_0-1725982066460.png

 

I used this Loader with STM32F429-EVAL board and it works well.

I don't think the error you are showing has a relation with the loader. 

Could you please share your project (in PV if you don't want to share it in public) so I can do a test?

 

2 replies

mƎALLEm
Technical Moderator
September 10, 2024

Hello,

Why did you duplicate this thread instead of replying in it? https://community.st.com/t5/stm32cubeide-mcus/external-loader-file-not-found/td-p/717263

Please don't duplicate the same topic.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
MuthamizhAuthor
Associate II
September 10, 2024

Okay but i need better visibility to my problem i don't find any stldr file for my stm32f429i series.

could u please look into it to solve the issues.  :)

Note: I had also tried the solution u had suggested for this previously.

mƎALLEm
mƎALLEmBest answer
Technical Moderator
September 10, 2024

@Muthamizh wrote:

 i don't find any stldr file for my stm32f429i series.


How? any loader? already provided you one.

Also in the CubeProgrammer, this is the list of all loader available for this board. And the one in the red rectangle corresponds to the NOR Flash loader.

SofLit_0-1725982066460.png

 

I used this Loader with STM32F429-EVAL board and it works well.

I don't think the error you are showing has a relation with the loader. 

Could you please share your project (in PV if you don't want to share it in public) so I can do a test?

 

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
MuthamizhAuthor
Associate II
September 11, 2024

My board series is STM32F429I-DISC1 does the STM32F429-EVAL &STM32F429I-DISC1 are different or both functionality and all other specs are same.

mƎALLEm
Technical Moderator
September 11, 2024

There is no EXTERNAL Loader for STM32F429I-DISC1.

Whey in the previous post you are looking for an external loader? I thought you are using an EVAL board.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
MuthamizhAuthor
Associate II
September 11, 2024

Okay how can I use IDE to work with this board do you have any idea.