Debugging program in external flash XIP mode STM32N6
Hi,
I am trying to debug STM32N6 program loaded in external flash. When I started the debugger in the FSBL project I can put a breakpoint just before it jumps into application inside external flash. It is obvious I wont be able to see the symbols since it is not loaded. So I loaded my application elf file under debug_configuration/Startup/Load Image and Symbols (See attached image). When I start my debugging session, I encounter the following error and was unable to debug even FSBL code.
Board: STM32N6 DK
STM32CubeIDE: 1.17.0
Platform: Window
project: Template_XIP_FSBL (found under Stcube package for N6).
Here is the error:
STMicroelectronics ST-LINK GDB server. Version 7.9.0
Copyright (c) 2024, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Failed to read all registers from target
Failed to read all registers from target
Failed to read all registers from target
Failed to read all registers from target
Thanks