Skip to main content
Bouzid-s
Associate
September 20, 2024
Solved

Debugging Works Manually, But Not from STM32CubeIDE (ST-Link GDB Server Issue)

  • September 20, 2024
  • 3 replies
  • 3554 views

 

Hi everyone,

I'm facing an issue with debugging STM32 projects in STM32CubeIDE. I'm using a MacBook Pro with an M3 ARM CPU and debugging an STM32 project using the ST-Link GDB server. When I manually run the ST-Link GDB server from the terminal with the appropriate command, everything works fine. However, when I attempt to start the debugging session directly from the Debug button in STM32CubeIDE, it doesn't work.

Detailed Issue:

  • STM32CubeIDE Version: ( STM32CubeIDE 1.16.1)
  • Target Microcontroller: ( STM32 Nucleo_G431KB )
  • Debugger: ST-Link (i tried openOCD and GDB) and J-link (Segger)
  • Host System: macbook pro  M3 ARM CPU)

Manual Debugging Command:

When I run the following command in the external terminal, the GDB server starts properly, and I'm able to debug the application. I use then remote GDB server (localhost with default port)

 
/Applications/STM32CubeIDE.app/Contents/Eclipse/plugins/com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.macos64_2.1.400.202404281720/tools/bin/ST-LINK_gdbserver -cp /Applications/STMicroelectronics/STM32Cube/STM32CubeProgrammer/STM32CubeProgrammer.app/Contents/MacOs/bin/STM32_Programmer_CLI /Users/bouzid-s/STM32CubeIDE/workspace_1.16.1/Blink_Led/Debug/Blink_Led.elf

This starts the GDB server and loads my application without any issues.

Problem with STM32CubeIDE Debugging:

However, when I click the Debug button in STM32CubeIDE to launch the debugging session, it fails to work. The exact behavior is that the IDE either does not start the GDB server correctly or there’s a mismatch in the way the debugger is configured internally. I've tried the following approaches:

What I Need Help With:

  • Is there a known issue with the ST-Link GDB server integration in STM32CubeIDE on macOS that could cause this behavior?
  • Is there a specific configuration or workaround that allows the IDE to launch the GDB server correctly without requiring manual intervention?

Any advice on how to resolve this issue so I can debug directly from STM32CubeIDE would be greatly appreciated!

Thanks in advance for your help.

Best regards,

    3 replies

    Andrew Neil
    Andrew NeilBest answer
    Super User
    September 20, 2024
    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Bouzid-s
    Bouzid-sAuthor
    Associate
    September 25, 2024

    Yes. Thanks ! Runing CubeIDE as sudoer should solve my problem for now.

    Semer CHERNI
    ST Employee
    September 25, 2024

    Hello @Bouzid-s 

    First thanks for posting.

    As @Andrew Neil asked, are you using the macOS 15?

    Also could you provide the complete debug log?

    BR,
    Semer.

    Explorer
    September 29, 2024

    Try what emrys57 did on this link:

    https://stackoverflow.com/questions/78996974/stm32cubeide-debugger-no-longer-works-in-macos-15-0-sequoia 

    and it seems to work the debug session, so check it out!

    Kind regards