Skip to main content
Associate III
May 9, 2025
Question

Flash Test for STM32H735 using CLASS B firmware

  • May 9, 2025
  • 1 reply
  • 727 views

I have downloaded the "STM32CubeExpansion_CLASSB_H7_V4.0.0" to Falsh test(CRC) as per given in UM3252 user manual . In the UM3252, I have gone through "5.5.2 Steps to build an application from scratch" to do flash test for my project .I am using the STM32cube IDE to integrate CLASSB firmware to my project. I have encountered the following problems.

1.I am unable to found the CRC tool in STM32cube programmer which is given in UM3252. Where can i found the CRC tool?

2.I have added and compiled successfully the SRC an INC to my project from given firmware ...Middleware\ST\STM32_Safety_STL. When i add linker file "STL_Lib_product_x1.a " to my project in MCU GCC Linker/Libraries in STM32cube IDE. Where ,which and how can i add the the object file located in LIB folder from ...Middleware\ST\STM32_Safety_STL?

3.Please guide me to do the flash test on STM32H735 using STM32cube IDE.

1 reply

Aziz BRIGUI
Technical Moderator
May 14, 2025

Hello @Deviprasad Bokkisam,

I will address the STM32CubeProgrammer part and try to suggest some actions for the STM32CubeIDE part. 

1- You should download STM32CubeProgrammer. You can find it under this link STM32CubeProg - STM32CubeProgrammer software for all STM32 - STMicroelectronics. This step is described here 

AzizBRIGUI_0-1747128319841.png

and the CLI to use is described here:

AzizBRIGUI_1-1747128346615.png

2- A way to do it in STM32CubeIDE should be through "Project properties>C/C++ build>Settings>Tool Settings>MCU GCC linker>Libraries>add". Make sure you add the correct library for your device following this recommendation:

AzizBRIGUI_0-1747212850119.png

Hope you find this helpful.

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate III
May 15, 2025

Hi Sir,

Thank you so much for reply.

1.I have added Library part successfully by adding a prefix : to library file in the above said path. If i didn't prefix : then the CubeIDE gives the error Library cannot find.

2.I have downloaded STM32CubeProgrammer v2.19.0. I am unable to understand the "6.2.2 CRC tool set-up" given by you(above picture) in figure8 IAR post build actions screenshot relation to STM32cube IDE. Where can i found the above screen sheet i.e is it part of STM32cube IDE or it is in separate application?

3.

3.Please guide me step by step to do the flash test successfully using STM32cube IDE ,IAR Workbench and CRC tool.

InsignificantBit
ST Employee
May 28, 2025

Hello, for the post-build command for STM32CubeIDE projects, please refer to the included example project for STM32CubeIDE. You will find the post-build-command configuration in STM32CubeIDE in Project->Settings->C/C++ Build->Settings->Build Steps.

 

As explained in the "CRC tool set-up" chapter in the UM3252, it will only work if your OS $PATH variable contains the path to the STM32CubeProgrammer, or rather the directory containing the STM32_Programmer_CLI executable.

If that is not your case, you will need to change the command to explicitly call the STM32_Programmer_CLI executable by its full path (eg. /full/path/to/stm32cubeprogrammer/bin/STM32_Programmer_CLI.exe instead of just STM32_Programmer_CLI.exe.

 

 

There is also version of STM32_Programmer_CLI packaged within the STM32CubeIDE installation. You can call it by using the STM32CubeIDE's internal environment variable $cubeide_cubeprogrammer_path.

The simplified command to call the packaged executable would then e.g. be:

${cubeide_cubeprogrammer_path}/STM32_Programmer_CLI.exe -sl ${CWD}/${BuildArtifactFileName} 0x08000000 0x08010000 0x400