Associate
February 26, 2024
Question
FreeRTOS and USB givers Hard Fault in H743 MCU
- February 26, 2024
- 3 replies
- 1508 views
Dear Sirs
I am having a problem using FreeRTOS and USB on H7 series MCU. The IDE gives “Hard Fault” when I debug the project. See image below.

The environments are :
STM32CubeIDE: Version: 1.14.0, Build: 19471_20231121_1200 (UTC)
Target: NUCLEO-H743ZI2
Enclosed herewith are the two “ioc” files.
FreeRTOS_USB1.ioc is for the project without initialization to the USB and it is working fine.
FreeRTOS_USB.ioc is for the project with the initialization to the USB and it is giving my Hard Fault.
Your help and assistance are highly appreciated.
Best Regards
Dr Reyah Abdula