Skip to main content
Associate III
November 23, 2025
Question

Freertos backtrace problem

  • November 23, 2025
  • 2 replies
  • 167 views

Hi,

STM32CubeIDE 2.0

fresh project

with

GNU Tool for STM32: 14.3.rel1 :

PKurz1_0-1763928039074.png

GNU Tool for STM32: 13.3.rel1

PKurz1_1-1763928147123.png

regards

2 replies

Technical Moderator
December 4, 2025

Hello @PKurz.1 

Could you please provide the name of the MCU, the FreeRTOS version, or attach your project for further investigation.

BR, Souhaib

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
mattias norlander
ST Employee
March 2, 2026

Hi @PKurz.1,

Spotted similar behavior in STM32CubeIDE for VS Code... Made me wonder what is the root-cause?! Then the team informed me about this thread from you. We are facing the same issue...

Screenshot 2026-03-02 at 08.43.35.png

As you can see the stack unwinding is a bit broken... showing multiple entried of pxPortInitialiseStack.

 

Google is your best friend... Found this post on FreeRTOS forum:

In a nutshell you can get a better (but not perfect behavior) by defining:

#define configTASK_RETURN_ADDRESS NULL

 

It seems that nobody have found the "perfect solution". I am not an expert on neither GCC/GDB nor FreeRTOS. Hence I took a pragmatic approach to try to find some work-arounds:

In STM32CubeIDE for VS Code I can easily switch different bundles that I want to use when compiling/debugging my project without hacking my environment. GDB and GCC is delivered as 2x different bundles. So I configured my FreeRTOS projects to build and debug the FreeRTOS application with these combinations of bundles:

  • Test1: GCC-13 + GDB-13   =    OK
  • Test2: GCC-13 + GDB-14   =    OK
  • Test3: GCC-14 + GDB-13   =    FAIL
  • Test4: GCC-14 + GDB-14   =    FAIL

It seems that GCC-14 is the common denominator in all casese where debug stack unwinding is "faling"?!

This seems to be an "up-stream" bug, should be solved "up-stream"...