Associate III
October 18, 2024
Question
Generating code for HTTPD in NUCLEO-H745ZI Board
- October 18, 2024
- 1 reply
- 2873 views
Hi Team,
"I am trying to configure an HTTP server on the Nucleo-H745ZIT6 board, which has two Cortex cores. I am using Cortex-M7 for this. After enabling HTTP in middleware inside LwIP, and generating the code, LwIP is placed inside the Cortex-M7 folder, but the HTTP code is generated outside of it. When compiling, I get an error saying 'fsdata.c: No such directory.' They are adding the HTTP image inside the HTTP folder, but I need to configure the resources configuration but not getting the option and I'm not sure how. Can you help me with this?"
i am using stmcubeide 1.15.1 software
Best Regards,
Gagan Gowda