Skip to main content
QLiu.6
Associate II
November 26, 2024
Question

How to use STLINK-V3 + remote OpenOCD to debug?

  • November 26, 2024
  • 0 replies
  • 2271 views

STM32CubeIDE
Version: 1.15.1
Build: 21094_20240412_1041 (UTC)
OS: Windows 10, v.10.0, x86_64 / win32
Java vendor: Eclipse Adoptium
Java runtime version: 17.0.8.1+1
Java version: 17.0.8.1

STLINK V3J15M6B5S1

 

At localhost, I can use "ST-LINK(OpenOCD)" to debug STM32H723ZG 

The config file:

# This is an NUCLEO-H723ZG board with a single STM32H723ZGTx chip
#
# Generated by STM32CubeIDE
# Take care that such file, as generated, may be overridden without any early notice. Please have a look to debug launch configuration setup(s)

source [find interface/stlink-dap.cfg]


set WORKAREASIZE 0x8000

transport select "dapdirect_swd"

set CHIPNAME STM32H723ZGTx
set BOARDNAME NUCLEO-H723ZG

# Enable debug when in low power modes
set ENABLE_LOW_POWER 1

# Stop Watchdog counters when halt
set STOP_WATCHDOG 1

# STlink Debug clock frequency
set CLOCK_FREQ 8000

# Reset configuration
# use hardware reset, connect under reset
# connect_assert_srst needed if low power mode application running (WFI...)
reset_config srst_only srst_nogate connect_assert_srst
set CONNECT_UNDER_RESET 1
set CORE_RESET 0

# ACCESS PORT NUMBER
set AP_NUM 0
# GDB PORT
set GDB_PORT 3333





# BCTM CPU variables

source [find target/stm32h7x.cfg]

 

I have a Raspi4B with STlinkV3 connected and make OpenOCD run. Raspi4B connect in same subnet by WiFi.

From the log, STlinkV3 connect to target successfully as it got "Cortex-M7 r1p2 processor detected". But when I run debug in STM32CudeIDE, I got error:

 

PixPin_2024-11-26_16-23-27.jpg

 

The logs from OpenOCD:

sudo openocd -f stlink.cfg
Open On-Chip Debugger 0.12.0+dev-01805-g133dd9d66 (2024-11-26-13:10)
Licensed under GNU GPL v2
For bug reports, read
 http://openocd.org/doc/doxygen/bugs.html
WARNING: interface/stlink-dap.cfg is deprecated, please switch to interface/stlink.cfg
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V3J15M6B5S1 (API v3) VID:PID 0483:3753
Info : Target voltage: 0.001595
Error: target voltage may be too low for reliable debugging
Info : Unable to match requested speed 1800 kHz, using 1000 kHz
Info : Unable to match requested speed 1800 kHz, using 1000 kHz
Info : clock speed 1000 kHz
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x6ba02477
Info : [STM32H723ZGTx.ap2] Examination succeed
Info : [STM32H723ZGTx.cpu0] Cortex-M7 r1p2 processor detected
Warn : [STM32H723ZGTx.cpu0] Erratum 3092511: Cortex-M7 can halt in an incorrect address when breakpoint and exception occurs simultaneously
Info : [STM32H723ZGTx.cpu0] The erratum 3092511 workaround will resume after an incorrect halt
Info : [STM32H723ZGTx.cpu0] target has 8 breakpoints, 4 watchpoints
Info : [STM32H723ZGTx.cpu0] Examination succeed
Info : [STM32H723ZGTx.ap2] gdb port disabled
Info : [STM32H723ZGTx.cpu0] starting gdb server on 3333
Info : Listening on port 3333 for gdb connections
Info : [STM32H723ZGTx.cpu0] external reset detected
Info : accepting 'gdb' connection on tcp/3333
Error: timed out while waiting for target halted
Error: [STM32H723ZGTx.cpu0] Execution of event gdb-attach failed:

Error: Failed to read memory at 0x5c001000
Error: auto_probe failed
Error: Connect failed. Consider setting up a gdb-attach event for the target to prepare target for GDB connect, or use 'gdb_memory_map disable'.
Error: attempted 'gdb' connection rejected
Info : Halt timed out, wake up GDB.

 

The config file "stlink.cfg" is mostly same. Only one line added:

bindto 0.0.0.0

to make OpenOCD can accept incoming from all network interfaces.

 

Stucked at this error and can not go on. Does anyone have the remote debug run?