Install STM32CubeIDE on Linux / OpenSuse 15.3
I try to install STM32CubeIDE on Linux / OpenSuse 15.3.
When downloading the latest RPM (1.7.0) I click "Get Latest", accept and then it automatically downloads the Linux Generic Installer.
How can I get the RPM? Can somebody confirm the problem?
Anyway, I then run the generic installer script and accept all license related points.
I get some error messages:
libusbx >= 1.0 is needed by st-stlink-server-2.0.2-3.x86_64
Problem: conflicting requests
- nothing provides libncurses.so.5 needed by st-stm32cubeide_1.7.0-1.7.0-10852_20210715_0634.x86_64
- nothing provides st-stlink-server needed by st-stm32cubeide_1.7.0-1.7.0-10852_20210715_0634.x86_64
(try to add '--skip-broken' to skip uninstallable packages)
Regarding libncurses:
~> rpm -qa | grep libncurses
libncurses6-6.1-lp152.7.67.x86_64
libncurses5-6.1-lp152.7.67.x86_64
libncurses 5 is installed. Why does the installer complain?
Regarding libusbx:
The home page of libusbx says it is superseeded by libusb and the latest release from libusbx is from 2014.
libusbx is not available for my distro as RPM any more.
Regarding stlink-server:
I downloaded the st-stlink-server-2.0.2-3.
When I try to install the RPM I get:
# rpm -Uvh st-stlink-server-2.0.2-3-linux-amd64.rpm
error: Failed dependencies:
libusbx >= 1.0 is needed by st-stlink-server-2.0.2-3.x86_64
The generic .install.sh installs fine, but the STM32CubeIDE installer still shows the same message.
Also, when I add the recommended option --skip-broken (message from the install script), then the install script says it does not know the option --skip-broken.
Quite many inconsistencies, can anybody please give a hint on how to install STM32CubeIDE ?
Thanks for any hints,
Torsten