Skip to main content
matt-crc
Senior III
February 27, 2025
Question

Is it possible for the IDE to highlight user code

  • February 27, 2025
  • 2 replies
  • 623 views

Hello,

Is it possible to highlight USER CODE from CubeMX code generation?  For example, highlight everything between these types of comments:

/* USER CODE BEGIN PM */
/* USER CODE END PM */

In a similar way that #ifdef / #endif blocks are highlighted?

If not currently available, can it be added the the CubeMX CubeIDE wishlist?

thanks

Matthew

2 replies

Pavel A.
Super User
February 28, 2025

This can be done as Eclipse editor add-on. Eclipse is opensource project, a lot of add-ons are available in its "marketplace" (Help-> Eclipse marketplace). Anyone can make add-ons or sponsor development of whatever they need or want.

Same with VS Code - a lot of add-ons exist for it.

 

Andrew Neil
Super User
February 28, 2025

Indeed.

But this would be a useful add-on for ST to provide - as these sections are their thing, and key to properly using their auto-generated code.

It is the cause of quite a few problems seen here ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
April 4, 2025
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.