Issues with datagenerated includes in makefile
Im new to C programming and even more, programming with a MCU. I have started a project and it was compilable for a while but suddenly, i ran into issues with include errors in data generated code. This is the error code:
02:16:11 **** Incremental Build of configuration Debug for project TSCU_ER26 ****
make -j7 all
arm-none-eabi-gcc "../Drivers/CMSIS/RTOS2/Template/cmsis_os1.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DDEBUG -DUSE_PWR_LDO_SUPPLY -DUSE_HAL_DRIVER -DSTM32H7A3xx -c -I../Core/Inc -I../Drivers/STM32H7xx_HAL_Driver/Inc -I../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/CMSIS/RTOS2/Template/cmsis_os1.d" -MT"Drivers/CMSIS/RTOS2/Template/cmsis_os1.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Drivers/CMSIS/RTOS2/Template/cmsis_os1.o"
arm-none-eabi-gcc "../Drivers/CMSIS/RTOS2/Source/os_systick.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DDEBUG -DUSE_PWR_LDO_SUPPLY -DUSE_HAL_DRIVER -DSTM32H7A3xx -c -I../Core/Inc -I../Drivers/STM32H7xx_HAL_Driver/Inc -I../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/CMSIS/RTOS2/Source/os_systick.d" -MT"Drivers/CMSIS/RTOS2/Source/os_systick.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Drivers/CMSIS/RTOS2/Source/os_systick.o"
arm-none-eabi-gcc "../Drivers/CMSIS/RTOS2/Source/os_tick_gtim.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DDEBUG -DUSE_PWR_LDO_SUPPLY -DUSE_HAL_DRIVER -DSTM32H7A3xx -c -I../Core/Inc -I../Drivers/STM32H7xx_HAL_Driver/Inc -I../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/CMSIS/RTOS2/Source/os_tick_gtim.d" -MT"Drivers/CMSIS/RTOS2/Source/os_tick_gtim.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Drivers/CMSIS/RTOS2/Source/os_tick_gtim.o"
arm-none-eabi-gcc "../Drivers/CMSIS/RTOS2/Source/os_tick_ptim.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DDEBUG -DUSE_PWR_LDO_SUPPLY -DUSE_HAL_DRIVER -DSTM32H7A3xx -c -I../Core/Inc -I../Drivers/STM32H7xx_HAL_Driver/Inc -I../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/CMSIS/RTOS2/Source/os_tick_ptim.d" -MT"Drivers/CMSIS/RTOS2/Source/os_tick_ptim.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Drivers/CMSIS/RTOS2/Source/os_tick_ptim.o"
arm-none-eabi-gcc "../Drivers/CMSIS/NN/Source/SoftmaxFunctions/arm_softmax_q15.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DDEBUG -DUSE_PWR_LDO_SUPPLY -DUSE_HAL_DRIVER -DSTM32H7A3xx -c -I../Core/Inc -I../Drivers/STM32H7xx_HAL_Driver/Inc -I../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/CMSIS/NN/Source/SoftmaxFunctions/arm_softmax_q15.d" -MT"Drivers/CMSIS/NN/Source/SoftmaxFunctions/arm_softmax_q15.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Drivers/CMSIS/NN/Source/SoftmaxFunctions/arm_softmax_q15.o"
arm-none-eabi-gcc "../Drivers/CMSIS/NN/Source/SoftmaxFunctions/arm_softmax_q7.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DDEBUG -DUSE_PWR_LDO_SUPPLY -DUSE_HAL_DRIVER -DSTM32H7A3xx -c -I../Core/Inc -I../Drivers/STM32H7xx_HAL_Driver/Inc -I../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/CMSIS/NN/Source/SoftmaxFunctions/arm_softmax_q7.d" -MT"Drivers/CMSIS/NN/Source/SoftmaxFunctions/arm_softmax_q7.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Drivers/CMSIS/NN/Source/SoftmaxFunctions/arm_softmax_q7.o"
arm-none-eabi-gcc "../Drivers/CMSIS/NN/Source/PoolingFunctions/arm_pool_q7_HWC.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DDEBUG -DUSE_PWR_LDO_SUPPLY -DUSE_HAL_DRIVER -DSTM32H7A3xx -c -I../Core/Inc -I../Drivers/STM32H7xx_HAL_Driver/Inc -I../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/CMSIS/NN/Source/PoolingFunctions/arm_pool_q7_HWC.d" -MT"Drivers/CMSIS/NN/Source/PoolingFunctions/arm_pool_q7_HWC.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Drivers/CMSIS/NN/Source/PoolingFunctions/arm_pool_q7_HWC.o"
../Drivers/CMSIS/RTOS2/Source/os_tick_ptim.c:25:10: fatal error: RTE_Components.h: No such file or directory
25 | #include "RTE_Components.h"
| ^~~~~~~~~~~~~~~~~~
../Drivers/CMSIS/NN/Source/SoftmaxFunctions/arm_softmax_q7.c:31:10: fatal error: arm_math.h: No such file or directory
31 | #include "arm_math.h"
| ^~~~~~~~~~~~
../Drivers/CMSIS/NN/Source/PoolingFunctions/arm_pool_q7_HWC.c:31:10: fatal error: arm_math.h: No such file or directory
31 | #include "arm_math.h"
| ^~~~~~~~~~~~
../Drivers/CMSIS/RTOS2/Source/os_tick_gtim.c:25:10: fatal error: os_tick.h: No such file or directory
25 | #include "os_tick.h"
| ^~~~~~~~~~~
../Drivers/CMSIS/RTOS2/Source/os_systick.c:25:10: fatal error: os_tick.h: No such file or directory
25 | #include "os_tick.h"
| ^~~~~~~~~~~
../Drivers/CMSIS/NN/Source/SoftmaxFunctions/arm_softmax_q15.c:31:10: fatal error: arm_math.h: No such file or directory
31 | #include "arm_math.h"
| ^~~~~~~~~~~~
compilation terminated.
compilation terminated.
compilation terminated.
compilation terminated.
compilation terminated.
compilation terminated.
make: *** [Drivers/CMSIS/NN/Source/SoftmaxFunctions/subdir.mk:22: Drivers/CMSIS/NN/Source/SoftmaxFunctions/arm_softmax_q15.o] Error 1
make: *** Waiting for unfinished jobs....
make: *** [Drivers/CMSIS/RTOS2/Source/subdir.mk:25: Drivers/CMSIS/RTOS2/Source/os_tick_gtim.o] Error 1
make: *** [Drivers/CMSIS/NN/Source/PoolingFunctions/subdir.mk:19: Drivers/CMSIS/NN/Source/PoolingFunctions/arm_pool_q7_HWC.o] Error 1
make: *** [Drivers/CMSIS/RTOS2/Source/subdir.mk:25: Drivers/CMSIS/RTOS2/Source/os_systick.o] Error 1
make: *** [Drivers/CMSIS/RTOS2/Source/subdir.mk:25: Drivers/CMSIS/RTOS2/Source/os_tick_ptim.o] Error 1
make: *** [Drivers/CMSIS/NN/Source/SoftmaxFunctions/subdir.mk:22: Drivers/CMSIS/NN/Source/SoftmaxFunctions/arm_softmax_q7.o] Error 1
In file included from ../Drivers/CMSIS/RTOS2/Template/cmsis_os1.c:28:
../Drivers/CMSIS/RTOS2/Template/cmsis_os.h:157:10: fatal error: cmsis_os2.h: No such file or directory
157 | #include "cmsis_os2.h"
| ^~~~~~~~~~~~~
compilation terminated.
make: *** [Drivers/CMSIS/RTOS2/Template/subdir.mk:19: Drivers/CMSIS/RTOS2/Template/cmsis_os1.o] Error 1
"make -j7 all" terminated with exit code 2. Build might be incomplete.
02:16:12 Build Failed. 15 errors, 0 warnings. (took 1s.487ms)I will include my makefile, because i think its relevant:
################################################################################
# Automatically-generated file. Do not edit!
# Toolchain: GNU Tools for STM32 (13.3.rel1)
################################################################################
-include ../makefile.init
RM := rm -rf
# All of the sources participating in the build are defined here
-include sources.mk
-include Drivers/STM32H7xx_HAL_Driver/Src/subdir.mk
-include Drivers/CMSIS/RTOS2/Template/subdir.mk
-include Drivers/CMSIS/RTOS2/Source/subdir.mk
-include Drivers/CMSIS/NN/Source/SoftmaxFunctions/subdir.mk
-include Drivers/CMSIS/NN/Source/PoolingFunctions/subdir.mk
-include Drivers/CMSIS/NN/Source/NNSupportFunctions/subdir.mk
-include Drivers/CMSIS/NN/Source/FullyConnectedFunctions/subdir.mk
-include Drivers/CMSIS/NN/Source/ConvolutionFunctions/subdir.mk
-include Drivers/CMSIS/NN/Source/ActivationFunctions/subdir.mk
-include Drivers/CMSIS/NN/NN_Lib_Tests/nn_test/Ref_Implementations/subdir.mk
-include Drivers/CMSIS/NN/NN_Lib_Tests/nn_test/RTE/Device/STM32F411RETx/subdir.mk
-include Drivers/CMSIS/NN/NN_Lib_Tests/nn_test/RTE/Device/ARMCM7_SP/subdir.mk
-include Drivers/CMSIS/NN/NN_Lib_Tests/nn_test/RTE/Device/ARMCM4_FP/subdir.mk
-include Drivers/CMSIS/NN/NN_Lib_Tests/nn_test/RTE/Device/ARMCM4/subdir.mk
-include Drivers/CMSIS/NN/NN_Lib_Tests/nn_test/RTE/Device/ARMCM3/subdir.mk
-include Drivers/CMSIS/NN/NN_Lib_Tests/nn_test/RTE/Device/ARMCM0/subdir.mk
-include Drivers/CMSIS/NN/Examples/ARM/arm_nn_examples/gru/RTE/Device/ARMCM7_SP/subdir.mk
-include Drivers/CMSIS/NN/Examples/ARM/arm_nn_examples/gru/RTE/Device/ARMCM4_FP/subdir.mk
-include Drivers/CMSIS/NN/Examples/ARM/arm_nn_examples/gru/RTE/Device/ARMCM3/subdir.mk
-include Drivers/CMSIS/NN/Examples/ARM/arm_nn_examples/gru/RTE/Device/ARMCM0/subdir.mk
-include Drivers/CMSIS/NN/Examples/ARM/arm_nn_examples/cifar10/RTE/Device/ARMCM7_SP/subdir.mk
-include Drivers/CMSIS/NN/Examples/ARM/arm_nn_examples/cifar10/RTE/Device/ARMCM4_FP/subdir.mk
-include Drivers/CMSIS/NN/Examples/ARM/arm_nn_examples/cifar10/RTE/Device/ARMCM3/subdir.mk
-include Drivers/CMSIS/NN/Examples/ARM/arm_nn_examples/cifar10/RTE/Device/ARMCM0/subdir.mk
-include Drivers/CMSIS/DSP/Source/TransformFunctions/subdir.mk
-include Drivers/CMSIS/DSP/Source/SupportFunctions/subdir.mk
-include Drivers/CMSIS/DSP/Source/StatisticsFunctions/subdir.mk
-include Drivers/CMSIS/DSP/Source/MatrixFunctions/subdir.mk
-include Drivers/CMSIS/DSP/Source/FilteringFunctions/subdir.mk
-include Drivers/CMSIS/DSP/Source/FastMathFunctions/subdir.mk
-include Drivers/CMSIS/DSP/Source/ControllerFunctions/subdir.mk
-include Drivers/CMSIS/DSP/Source/ComplexMathFunctions/subdir.mk
-include Drivers/CMSIS/DSP/Source/CommonTables/subdir.mk
-include Drivers/CMSIS/DSP/Source/BasicMathFunctions/subdir.mk
-include Drivers/CMSIS/DSP/PythonWrapper/cmsisdsp_pkg/src/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_variance_example/RTE/Device/ARMCM7_SP/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_variance_example/RTE/Device/ARMCM4_FP/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_variance_example/RTE/Device/ARMCM3/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_variance_example/RTE/Device/ARMCM0/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_variance_example/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_sin_cos_example/RTE/Device/ARMCM7_SP/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_sin_cos_example/RTE/Device/ARMCM4_FP/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_sin_cos_example/RTE/Device/ARMCM3/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_sin_cos_example/RTE/Device/ARMCM0/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_sin_cos_example/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_signal_converge_example/RTE/Device/ARMCM7_SP/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_signal_converge_example/RTE/Device/ARMCM4_FP/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_signal_converge_example/RTE/Device/ARMCM3/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_signal_converge_example/RTE/Device/ARMCM0/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_signal_converge_example/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_matrix_example/RTE/Device/ARMCM7_SP/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_matrix_example/RTE/Device/ARMCM4_FP/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_matrix_example/RTE/Device/ARMCM3/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_matrix_example/RTE/Device/ARMCM0/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_matrix_example/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_linear_interp_example/RTE/Device/ARMCM7_SP/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_linear_interp_example/RTE/Device/ARMCM4_FP/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_linear_interp_example/RTE/Device/ARMCM3/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_linear_interp_example/RTE/Device/ARMCM0/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_linear_interp_example/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_graphic_equalizer_example/RTE/Device/ARMCM7_SP/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_graphic_equalizer_example/RTE/Device/ARMCM4_FP/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_graphic_equalizer_example/RTE/Device/ARMCM3/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_graphic_equalizer_example/RTE/Device/ARMCM0/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_graphic_equalizer_example/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_fir_example/RTE/Device/ARMCM7_SP/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_fir_example/RTE/Device/ARMCM4_FP/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_fir_example/RTE/Device/ARMCM3/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_fir_example/RTE/Device/ARMCM0/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_fir_example/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_fft_bin_example/RTE/Device/ARMCM7_SP/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_fft_bin_example/RTE/Device/ARMCM4_FP/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_fft_bin_example/RTE/Device/ARMCM3/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_fft_bin_example/RTE/Device/ARMCM0/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_fft_bin_example/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_dotproduct_example/RTE/Device/ARMCM7_SP/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_dotproduct_example/RTE/Device/ARMCM4_FP/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_dotproduct_example/RTE/Device/ARMCM3/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_dotproduct_example/RTE/Device/ARMCM0/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_dotproduct_example/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_convolution_example/RTE/Device/ARMCM7_SP/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_convolution_example/RTE/Device/ARMCM4_FP/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_convolution_example/RTE/Device/ARMCM3/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_convolution_example/RTE/Device/ARMCM0/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_convolution_example/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_class_marks_example/RTE/Device/ARMCM7_SP/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_class_marks_example/RTE/Device/ARMCM4_FP/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_class_marks_example/RTE/Device/ARMCM3/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_class_marks_example/RTE/Device/ARMCM0/subdir.mk
-include Drivers/CMSIS/DSP/Examples/ARM/arm_class_marks_example/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/RefLibs/src/TransformFunctions/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/RefLibs/src/SupportFunctions/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/RefLibs/src/StatisticsFunctions/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/RefLibs/src/MatrixFunctions/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/RefLibs/src/Intrinsics/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/RefLibs/src/HelperFunctions/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/RefLibs/src/FilteringFunctions/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/RefLibs/src/FastMathFunctions/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/RefLibs/src/ControllerFunctions/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/RefLibs/src/ComplexMathFunctions/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/RefLibs/src/BasicMathFunctions/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/DspLibTest_FVP_A5/RTE/Device/ARMCA5/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/DspLibTest_FVP_A5/RTE/CMSIS/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/DspLibTest_FVP_A5/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/Common/src/transform_tests/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/Common/src/support_tests/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/Common/src/statistics_tests/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/Common/src/matrix_tests/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/Common/src/intrinsics_tests/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/Common/src/filtering_tests/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/Common/src/fast_math_tests/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/Common/src/controller_tests/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/Common/src/complex_math_tests/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/Common/src/basic_math_tests/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/Common/src/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/Common/platform/GCC/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/Common/platform/ARMCLANG/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/Common/platform/ARMCC/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/Common/platform/subdir.mk
-include Drivers/CMSIS/DSP/DSP_Lib_TestSuite/Common/JTest/src/subdir.mk
-include Drivers/CMSIS/Core_A/Source/subdir.mk
-include Drivers/CMSIS/Core/Template/ARMv8-M/subdir.mk
-include Core/Startup/subdir.mk
-include Core/Src/tscu/subdir.mk
-include Core/Src/subdir.mk
-include objects.mk
ifneq ($(MAKECMDGOALS),clean)
ifneq ($(strip $(S_DEPS)),)
-include $(S_DEPS)
endif
ifneq ($(strip $(S_UPPER_DEPS)),)
-include $(S_UPPER_DEPS)
endif
ifneq ($(strip $(C_DEPS)),)
-include $(C_DEPS)
endif
endif
-include ../makefile.defs
OPTIONAL_TOOL_DEPS := \
$(wildcard ../makefile.defs) \
$(wildcard ../makefile.init) \
$(wildcard ../makefile.targets) \
BUILD_ARTIFACT_NAME := TSCU_ER26
BUILD_ARTIFACT_EXTENSION := elf
BUILD_ARTIFACT_PREFIX :=
BUILD_ARTIFACT := $(BUILD_ARTIFACT_PREFIX)$(BUILD_ARTIFACT_NAME)$(if $(BUILD_ARTIFACT_EXTENSION),.$(BUILD_ARTIFACT_EXTENSION),)
# Add inputs and outputs from these tool invocations to the build variables
EXECUTABLES += \
TSCU_ER26.elf \
MAP_FILES += \
TSCU_ER26.map \
SIZE_OUTPUT += \
default.size.stdout \
OBJDUMP_LIST += \
TSCU_ER26.list \
# All Target
all: main-build
# Main-build Target
main-build: TSCU_ER26.elf secondary-outputs
# Tool invocations
TSCU_ER26.elf TSCU_ER26.map: $(OBJS) $(USER_OBJS) /Users/anton/Formula/tscu_er26/STM32H7A3VITX_FLASH.ld makefile objects.list $(OPTIONAL_TOOL_DEPS)
arm-none-eabi-gcc -o "TSCU_ER26.elf" @"objects.list" $(USER_OBJS) $(LIBS) -mcpu=cortex-m7 -T"/Users/anton/Formula/tscu_er26/STM32H7A3VITX_FLASH.ld" --specs=nosys.specs -Wl,-Map="TSCU_ER26.map" -Wl,--gc-sections -static --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -Wl,--end-group
@echo 'Finished building target: $@'
@echo ' '
default.size.stdout: $(EXECUTABLES) makefile objects.list $(OPTIONAL_TOOL_DEPS)
arm-none-eabi-size $(EXECUTABLES)
@echo 'Finished building: $@'
@echo ' '
TSCU_ER26.list: $(EXECUTABLES) makefile objects.list $(OPTIONAL_TOOL_DEPS)
arm-none-eabi-objdump -h -S $(EXECUTABLES) > "TSCU_ER26.list"
@echo 'Finished building: $@'
@echo ' '
# Other Targets
clean:
-$(RM) TSCU_ER26.elf TSCU_ER26.list TSCU_ER26.map default.size.stdout
-@echo ' '
secondary-outputs: $(SIZE_OUTPUT) $(OBJDUMP_LIST)
fail-specified-linker-script-missing:
@echo 'Error: Cannot find the specified linker script. Check the linker settings in the build configuration.'
@exit 2
warn-no-linker-script-specified:
@echo 'Warning: No linker script specified. Check the linker settings in the build configuration.'
.PHONY: all clean dependents main-build fail-specified-linker-script-missing warn-no-linker-script-specified
-include ../makefile.targets
As i said, I'm new to this so if this is a basic or "unnecessary" question to ask, just point me in the right direction. I have searched through other issues and posts but I haven't found anything of help. If there is another post with a solution, point me in that direction. Thank you for your help beforehand!