J-Link: Live expression do not work after upgrade to STM32CubeIDE 2.1.0
Title edited to indicate that this is specific to J-Link.
Hi,
After updating to STM32CubeIDE 2.1.0 I get the following message after starting a debug session. Live expressions do not work.

From the console:
SEGGER J-Link GDB Server V9.14a Command Line Version
JLinkARM.dll V9.14a (DLL compiled Jan 28 2026 17:11:52)
Command line: -port 2331 -s -device STM32F769NI -endian little -speed 4000 -if swd -swoport 2332 -vd -rtos C:\ST\STM32CubeIDE_1.11.2\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.jlink.win32_2.5.200.202601091506\tools\bin\GDBServer\RTOSPlugin_FreeRTOS.dll
-----GDB Server start settings-----
GDBInit file: none
GDB Server Listening port: 2331
SWO raw output listening port: 2332
Terminal I/O port: 2333
Accept remote connection: localhost only
Generate logfile: off
Verify download: on
Init regs on start: off
Silent mode: off
Single run mode: on
Target connection timeout: 0 ms
------J-Link related settings------
J-Link Host interface: USB
J-Link script: none
J-Link settings file: none
------Target related settings------
Target device: STM32F769NI
Target device parameters: none
Target interface: SWD
Target interface speed: 4000kHz
Target endian: little
Connecting to J-Link...
J-Link is connected.
Firmware: J-Trace PRO V2 Cortex-M compiled Dec 4 2024 17:58:04
Hardware: V2.00
S/N: 752000803
Feature(s): RDI, FlashBP, FlashDL, JFlash, GDB
Checking target voltage...
Target voltage: 3.33 V
Listening on TCP/IP port 2331
Connecting to target...
Halting core...
Connected to target
The debug settings: