Question
Linux installation error
d64.deb'
Note, selecting 'st-stlink-udev-rules' instead of './st-stlink-udev-rules-1.0.3-2-linux-all.deb'
Note, selecting 'st-stm32cubeide-1.15.1' instead of './st-stm32cubeide-1.15.1-21094-20240412-1041_amd64.deb'
Note, selecting 'segger-jlink-udev-rules' instead of './segger-jlink-udev-rules-7.94h-linux-all.deb'
Some packages could not be installed. This may mean that you have
requested an impossible situation or if you are using the unstable
distribution that some required packages have not yet been created
or been moved out of Incoming.
The following information may help to resolve the situation:
The following packages have unmet dependencies:
st-stm32cubeide-1.15.1 : Depends: libncurses5 but it is not installable
Depends: libpython2.7 but it is not installable
Depends: libwebkit2gtk-4.0-37 but it is not installable
E: Unable to correct problems, you have held broken packages.
Which STM32IDE we should download to fix this error