Missing 'External loaders' in Debugger tab
Hello,
I've recently created an External Loader to be used on a TouchGFX project (H563 with SPI LCD and SPI external flash). When I use this loader in Cube Programmer, it programs the processor and SPI flash, and runs as expected. So now I want to add it into my project in CubeIDE. Normally I would find the External Loaders under the Debugger tab (between SWV and Misc) but this seems to be missing. Is there a way to enable this?

(This project was created un der CubeIDE 2.0.0, but this section also is missing in projects created by previous versions. Example projects created from TouchGFX does have this section).
Any ideas?
PP22