Skip to main content
Son, Dong-Seong
Associate III
May 16, 2025
Question

Prevent Flash Erase of EEPROM Pages During STM32CubeIDE Download

  • May 16, 2025
  • 1 reply
  • 711 views

Hello,

I am using an STM32F103VCT microcontroller and the EEPROM emulation library. I write data with the EE_WriteVariable() function and read it back with EE_ReadVariable(). However, whenever I download new firmware to the MCU via ST-Link V2 in STM32CubeIDE, the entire flash memory is erased—including the regions where I stored data using EE_WriteVariable().

Is there any way to download or debug new firmware without erasing the flash pages used by the EEPROM emulation?

For reference, I’m running STM32CubeIDE version 1.18.1. Any suggestions would be greatly appreciated.

Thank you!

1 reply

Andrew Neil
Super User
May 16, 2025
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Son, Dong-Seong
Associate III
May 16, 2025

Hi Andrew

thank you for your reponse.

Below is all of the code I’m using with the EEPROM emulation library. Are there any parts here that could be causing problems?

I would greatly appreciate it if you could let me know how to resolve this.

 

void read_eeprom()
{
EE_ReadVariable (0x0001, (uint16_t*)&gstSystem.nNumOfBlock);

EE_ReadVariable (0x0002, (uint16_t*)&gstMain.stRep.nInputVccMax);
EE_ReadVariable (0x0003, (uint16_t*)&gstMain.stRep.nInputVccMin);
EE_ReadVariable (0x0004, (uint16_t*)&gstMain.stRep.bBiastInOn);
EE_ReadVariable (0x0005, (uint16_t*)&gstMain.stRep.bBiastOut1On);
EE_ReadVariable (0x0006, (uint16_t*)&gstMain.stRep.bBiastOut2On);
EE_ReadVariable (0x0007, (uint16_t*)&gstMain.stRep.nTempMax);
EE_ReadVariable (0x0008, (uint16_t*)&gstMain.stRep.bShutdownOn);
EE_ReadVariable (0x0009, (uint16_t*)&gstMain.stRep.bAmpOn);
EE_ReadVariable (0x0010, (uint16_t*)&gstMain.stRep.bAlcOn);
EE_ReadVariable (0x0011, (uint16_t*)&gstMain.stRep.nOutputLevelMax);
EE_ReadVariable (0x0012, (uint16_t*)&gstMain.stRep.nAlcLevel);
EE_ReadVariable (0x0013, (uint16_t*)&gstMain.stRep.nAttenIn);
EE_ReadVariable (0x0014, (uint16_t*)&gstMain.stRep.nAttenOut);
EE_ReadVariable (0x0015, (uint16_t*)&gstMain.stRep.nAttenL1);
EE_ReadVariable (0x0016, (uint16_t*)&gstMain.stRep.nAttenL2);
}

void write_eeprom()
{
HAL_FLASH_Unlock();
EE_WriteVariable (0x0001, gstSystem.nNumOfBlock);

EE_WriteVariable (0x0002, gstMain.stRep.nInputVccMax);
EE_WriteVariable (0x0003, gstMain.stRep.nInputVccMin);
EE_WriteVariable (0x0004, gstMain.stRep.bBiastInOn);
EE_WriteVariable (0x0005, gstMain.stRep.bBiastOut1On);
EE_WriteVariable (0x0006, gstMain.stRep.bBiastOut2On);
EE_WriteVariable (0x0007, gstMain.stRep.nTempMax);
EE_WriteVariable (0x0008, gstMain.stRep.bShutdownOn);
EE_WriteVariable (0x0009, gstMain.stRep.bAmpOn);
EE_WriteVariable (0x0010, gstMain.stRep.bAlcOn);
EE_WriteVariable (0x0011, gstMain.stRep.nOutputLevelMax);
EE_WriteVariable (0x0012, gstMain.stRep.nAlcLevel);
EE_WriteVariable (0x0013, gstMain.stRep.nAttenIn);
EE_WriteVariable (0x0014, gstMain.stRep.nAttenOut);
EE_WriteVariable (0x0015, gstMain.stRep.nAttenL1);
EE_WriteVariable (0x0016, gstMain.stRep.nAttenL2);
HAL_FLASH_Lock();
}

void read_eeprom_table(uint8_t sel)
{
if(sel >= 2) return;

int pos = 40;

EE_ReadVariable (pos + 0, (uint16_t*)&gstTable[sel].nItem);
EE_ReadVariable (pos + 1, (uint16_t*)&gstTable[sel].step);
EE_ReadVariable (pos + 2, (uint16_t*)&gstTable[sel].max_val);

for(int i=0; i<MAX_TABLE_ITEM_NO; i++) {
EE_ReadVariable (pos + 10 + i, (uint16_t*)&gstTable[sel].table[i]);
}

if(gstTable[sel].nItem == 0 || gstTable[sel].nItem > 100) {
gstTable[sel].nItem = 71;
gstTable[sel].step = 10;
gstTable[sel].max_val = 100;
}
}

void write_eeprom_table(uint8_t sel)
{
if(sel >= 2) return;

int pos = 40;

HAL_FLASH_Unlock();
EE_WriteVariable (pos + 0, gstTable[sel].nItem);
EE_WriteVariable (pos + 1, gstTable[sel].step);
EE_WriteVariable (pos + 2, gstTable[sel].max_val);

for(int i=0; i<MAX_TABLE_ITEM_NO; i++) {
EE_WriteVariable (pos + 10 + i, gstTable[sel].table[i]);
}

HAL_FLASH_Lock();
}

 

Andrew Neil
Super User
May 16, 2025

Please see How to insert source code - the indentation is all lost now, so you'll need to copy again from your original.

You can edit the post:

AndrewNeil_0-1747392633827.png

 

I don't see in that code where you set the location of your emulated EEPROM within the Flash ?

Also, how much of the Flash is used by your code?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.