SBSFU failing to find user firmware
Hi, we are trying to flash with keil mdk bin file and failing when validating user firmware. Below is the output from Tera Term.
= [SBOOT] System Security Check successfully passed. Starting...
======================================================================
= (C) COPYRIGHT 2017 STMicroelectronics =
= =
= Secure Boot and Secure Firmware Update =
======================================================================
= [SBOOT] SECURE ENGINE INITIALIZATION SUCCESSFUL
= [SBOOT] STATE: CHECK STATUS ON RESET
INFO: A Reboot has been triggered by a Hardware reset!
= [SBOOT] STATE: CHECK NEW FIRMWARE TO DOWNLOAD
= [SBOOT] STATE: CHECK KMS BLOB TO INSTALL
= [SBOOT] STATE: CHECK USER FW STATUS
A FW is detected in the slot SLOT_ACTIVE_1
= [SBOOT] STATE: VERIFY USER FW SIGNATURE
= [SBOOT] STATE: HANDLE CRITICAL FAILURE
= [SBOOT] STATE: REBOOT STATE MACHINE
========= End of Execution ==========
= [SBOOT] System Security Check successfully passed. Starting...
======================================================================
= (C) COPYRIGHT 2017 STMicroelectronics =
= =
= Secure Boot and Secure Firmware Update =
======================================================================
= [SBOOT] SECURE ENGINE INITIALIZATION SUCCESSFUL
= [SBOOT] STATE: CHECK STATUS ON RESET
INFO: A Reboot has been triggered by a Software reset!
= [SBOOT] STATE: CHECK NEW FIRMWARE TO DOWNLOAD
= [SBOOT] STATE: CHECK KMS BLOB TO INSTALL
= [SBOOT] STATE: CHECK USER FW STATUS
No valid FW found in the active slots nor new FW to be installed
Waiting for the local download to start...
= [SBOOT] STATE: DOWNLOAD NEW USER FIRMWARE
File> Transfer> YMODEM> Send ...........................................
It is waiting forever to download new user firmware, didn't have any issues until application firmware modified and being new to keil mdk, not able to figure out why application code changes disrupting memory mapping.
Below is the SCT file
#! armclang --target=arm-arm-none-eabi -mcpu=cortex-m0plus -E -xc
; *************************************************************
; *** Scatter-Loading Description File generated by uVision ***
; *************************************************************
#include "..\..\Linker_Common\MDK-ARM\mapping_sbsfu.h"
#include "..\..\Linker_Common\MDK-ARM\mapping_fwimg.h"
LR_IROM1 (SLOT_ACTIVE_1_START + 0x200) { ; load region size_region
; FLASH
vector_start (SLOT_ACTIVE_1_START + 0x200) FIXED VECTOR_SIZE {
*.o (RESET, +First)
}
ROM_region +0 {
*(InRoot$$Sections)
.ANY (+RO)
}
; NVM FLASH Data
; WARNING: Symbols not used. The NVMS address is defined in lora_app.c
; RW_LW_NVM_ROM 0x0803F000 0x00001000
; Non-backup SRAM1
RW_IRAM1 SB_REGION_RAM_START SB_RAM_REGION_SIZE { ; RW data
.ANY (+RW +ZI)
}
; NVM RAM Data
RW_LW_NVM_RAM LW_NVM_RAM_START UNINIT LW_NVM_RAM_REGION_SIZE { ; RW data
*(.bss.LW_NVM_RAM)
*(.bss.LW_NVM_BACKUP_RAM)
}
}
; extra ROM region to make sure the binary size is a multiple of the AES block size (16 bytes) and WL flash writing unit (8 bytes)
LR_ROM1(+0) ALIGN(16) {
ForAlignment +0 {
startup_stm32wl55xx_cm4.o (ALIGNTOAESBLOCK,+Last)
}
}
Any help or pointing in the right direction greatly appreciated.
Thanks