Skip to main content
Associate
September 17, 2024
Question

Search: An internal error occurred during: "File Search Worker".

  • September 17, 2024
  • 3 replies
  • 12512 views
When I execute a text search in the Stm32CubeIDE Version: 1.16.0
Build: 21983_20240628_1741 (UTC) the following error appears:
 
Problems encountered during text search.
An internal error occurred during: “File Search Worker”.
'byte[] org.eclipse.core.resources.IFile.readNBytes(int)'
 
The error log then reads:
!SUBENTRY 1 org.eclipse.core.jobs 4 2 2024-09-17 08:36:23.077
!MESSAGE An internal error occurred during: “File Search Worker”.
!STACK 0
java.lang.NoSuchMethodError: 'byte[] org.eclipse.core.resources.IFile.readNBytes(int)'
at org.eclipse.search.internal.core.text.FileCharSequenceProvider.toShortString(FileCharSequenceProvider.java:495)
at org.eclipse.search.internal.core.text.FileCharSequenceProvider.newCharSequence(FileCharSequenceProvider.java:42)
at org.eclipse.search.internal.core.text.TextSearchVisitor$TextSearchJob.processFile(TextSearchVisitor.java:208)
at org.eclipse.search.internal.core.text.TextSearchVisitor$TextSearchJob.run(TextSearchVisitor.java:173)
at org.eclipse.core.internal.jobs.Worker.run(Worker.java:63)
 
This error occurred suddenly
 
What can do to solve this Problem ?

3 replies

Visitor II
September 17, 2024

this started happening to me after installing a Copilot plugin from Eclipse marketplace.

Uninstalling the plugin didn't help.

I reinstalled eclipse and this fixed the problem.

Associate II
September 18, 2024

hi,

 

was it this one? https://marketplace.eclipse.org/content/copilot4eclipse

i have the same problem, also installed this plugin and it happened all of a sudden. for some time it did work. i did not change anything and *poff* i got this error

i have the same error in another eclipse based IDE (where i also installed this plugin)
in the beginning it worked flawlessly 

Associate
September 18, 2024

Ok, I had also installed the Copilot plugin. At the beginning everything worked and then yesterday suddenly this error message when searching.
Now I have reinstalled the CubeIde, but still without Copilot Plugin, at the moment the search function works again.

Semer CHERNI
ST Employee
September 25, 2024

Hello

Thanks for posting :).

The copilot plugin for Eclipse is not compatible with the Eclipse CDT version on which STM32CubeIDE is based.

The investigation is ongoing internally and it should be fixed when the Eclipse version used by STM32CubeIDE is upgraded. This will be included in future releases.

KR,
Semer.

Associate II
September 25, 2024

hi,

there was an update from Genuitec. This posting explains the details. With this version it should be fixed

https://github.com/Genuitec/Copilot4Eclipse-community/discussions/23