ST link error: Failed to bind to port 61235; Failure starting SWV server
Hi I am experiencing an issue on my IDE I couldn't able to Run/Debug .However the ST Link can be communicated with the target in STM32 Cube programmer but not in STM32 cube IDE.

Console Error:
STMicroelectronics ST-LINK GDB server. Version 7.7.0
Copyright (c) 2024, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Failed to bind to port 61235, error code -1: No error
Failure starting SWV server on TCP port: 61235
Failed to bind to port 61234, error code -1: No error
Failure starting GDB server: TCP port 61234 not available.
Shutting down...
Exit.
Can someone Please help me