Starting tools from CubeIDE take a long time on modern Linux distributions
Hello community,
Few days ago, some post linked to performance issue with STM32CubeIDE on Ubunto 24.04 and Debian testing [trixie] machines.
This is a known issue in ECLIPSE and was not causing issues for STM32CubeIDE, however with the new Linux distributions the problem occurs.
Temporary solution:
As a temporary solution there are two propositions:
- Make temporary changes for each STM32CubeIDE start.
set the hard limit in current terminal : ulimit -n -H 4096 - Make change for the entire system: edit /etc/security/limits.conf and add the line “username hard nofile 4096”
Long term solution:
The long-term solution will be the integration of the newest Eclipse version in STM32CubeIDE