Question
STM32CubeCLT 1.19.0 released
We are pleased to announce that the release 1.19.0 of STM32CubeCLT is available.
What is new in 1.19.0:
- Support for ST Arm Clang toolchain
- Maintenance of the previous version
- Updated in accordance with STM32CubeIDE v1.19.0
Main fixed issues in 1.19.0:
No fixed issue to report.
Know problems and limitations in 1.19.0:
- The user must specify the path of STM32CubeProgrammer/bin as argument when executing ST-LINK_gdbserver as shown in the example below:
ST-LINK_gdbserver.exe -cp/c/ST/STM32CubeCLT/STM32CubeCLT/STM32CubeProgrammer/bin
- For MAC OS no paths for "CLANG_GCC_CMSIS_COMPILER" and GCC_TOOLCHAIN_ROOT.
The workaround is the following
- Open terminal
- Then source the file /etc/profile
- Then re do the echo command on these two variables but we must use the same terminal
How to get STM32CubeCLT 1.19.0:
- Under this link