Question
STM32CubeIDE 1.16.1 released
STM32CubeIDE 1.16.1 was released on st.com as well as an in-tool update patch aligned with STM32CubeMX v6.12.1 that is available for download.
Main issues fixed in this minor release:
- Fixed issue when install OpenSTLinux MP2 plugin from OpenSTLinux releases Update Sites.
- Fixed issue on project creation using MP255 devices.
- Fixes related to the integrated STM32CubeMX
- [MP25] Major differences in the ST Boards Device Trees between MX and Embedded SW (EV and DK Board) ==> Aligned with STM32CubeMX 6.12.1
- Create Project for each MCU: Mcu STM32MP2xxxxxx is not supported
- Missing MMC registers in SFR view for MP13 berametal
- Some miss function in CubeIDE for MP13 baremetal (FreeRTOS)
- Fetch mp2 update site -Error found with Setup OpenSTLinux
- [G4][Zest] Update Stack values
- [G4 Zest] update the field Mcu.UserName for the Z parts to display the right name
Check the errata under this link for more details.
Where do I obtain STM32CubeIDE 1.16.1?
- For STM32CubeIDE 1.16.1: STM32CubeIDE - Integrated Development Environment for STM32 - STMicroelectronics
- Or update your current installation of STM32CubeIDE using: Help > Check for updates.