STM32CubeIDE 2.0.0 Linux debugging issues and windows order breaks Plasma 6
Hello,
I'm facing very strange issues with STM32CubeIDE 2.0.0 under Linux Debian Trixie/Forky.
I'm running Kernel 6.17.11+deb14-amd64 with Plasma 6.5.4, KDE Framework 6.20.0 and QT version 6.9.2 in Wayland.
First issue is with debugger. I can start the firmware in debugging mode, runs but after few "Step Into" and "Step Over" commands the debugger is getting stuck. I doesn't take any commands anymore.
If I use "Restart" or "Terminate" or "Terminate and Relaunch" is starting again and again I can use few times "Step Into" and "Step Over"
Second issue is with windows ordering after using for a while STM32CubeIDE: it breaks completely the windows orders under Plasma and the only solution is to logout and login back and restart all apps.
I didn't get this issue with any other apps, except STM32CubeIDE.