STM32CubeIDE creates MCU project even when selecting STM32F429I-Discovery
Hello,
I’m currently working with an STM32F429I-Discovery board and an MT9M001 camera module,
and my goal is to display the camera image on the built-in LCD (ILI9341) using LTDC + DMA2D + DCMI.
When I select STM32F429I-Discovery in the STM32CubeIDE “Board Selector” and create a new project,
the project is still generated as a regular MCU project (STM32F429ZIT6).
Because of this, the LTDC pins (such as PI9 and PI10) are not automatically assigned,
and I get red warnings or conflicts in the LTDC configuration.
In particular, I’m facing the following issues:
PA4: LTDC_VSYNC conflicts with DCMI_HSYNC
PC6: LTDC_HSYNC conflicts with DCMI_D0
Pins like PI9 (VSYNC) and PI10 (HSYNC) do not appear in the Pinout view at all
I also tried official examples such as DCMI_CaptureMode and LTDC_Display_2Layers,
but these are made for the STM324x9I-EVAL board,
and because the Discovery board has a different LCD and pin configuration,
I couldn’t get them to work properly.
I’m still a beginner with STM32 and currently learning through trial and error.
Because of the many conflicts and warnings in CubeIDE, I’m not confident whether my setup is correct.
So I’d like to ask:
Is there any way to make STM32CubeIDE recognize STM32F429I-Discovery as a board (not just as an MCU project)?
If not, how should I configure LTDC when pins like PI9/PI10 are not available on the Discovery board?
Are there any official or working examples that show how to display a camera image (e.g., MT9M001) on the built-in LCD of the F429I-Discovery?
Any advice or guidance would be greatly appreciated,
especially for those of us who are still beginners trying to make this setup work.
Thank you very much.