Associate III
July 15, 2024
Solved
STM32CubeIDE doesn't flash target before debugging
- July 15, 2024
- 5 replies
- 4208 views
Hello,
After updating STM32CubeIDE to version 1.16, starting a debugging session doesn't load program into the STM32L5 target and jumps directly to the reset Handler.
I tried programming the bin file using STM32CubeProgrammer and it works well.
However, erasing the FLASH using STM32CubeProgrammer and launching a debug session then reading back the FLASH using STM32CubeProgrammer shows that it's empty.
Im trying to load the program to the address 0x08020000, here is the memories definition.
/* Memories definition */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 192K
SRAM2 (xrw) : ORIGIN = 0x20030000, LENGTH = 64K
BOOTLOADER (rx) : ORIGIN = 0x08000000, LENGTH = 128K
FLASH (rx) : ORIGIN = 0x08020000, LENGTH = 352K
}