STM32CubeIDE: HSI → PLL /2 not honored (Nucleo-F303RE, expected 36 MHz but runs at 72 MHz)
Hi Team,
I’m prototyping on a Nucleo-F303RE using STM32CubeIDE. In the clock configuration, I set the system clock to 36 MHz from HSI (HSI → PLL with the /2 divider), as shown in the clock tree screenshot.

However, my firmware misbehaved. After debugging, I found that SystemClock_Config() function isn’t applying the HSI/2 divider when feeding the PLL. Instead of:
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;CubeIDE generates:
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI_DIV2;
This effectively makes the system clock 72 MHz instead of the configured 36 MHz.
Did I misconfigure something in the clock setup, or is this a CubeIDE code-generation bug when using HSI with the PLL /2 divider?