STM32F767ZI - "Permission Denied" Compilation Error After Enabling Ethernet (LwIP)
Hello,
I’m working with the STM32F767ZI board and have configured Ethernet (ETH) peripheral with LwIP middleware using STM32CubeIDE. After generating the code and trying to compile the project, I encounter the following error:
This issue started occurring only after enabling the Ethernet peripheral and LwIP middleware. Prior to this configuration, the project was compiling successfully.
Steps Taken:
Enabled ETH in RMII mode
Enabled LwIP with default settings (static IP)
Generated code using STM32CubeMX
Tried cleaning and rebuilding the project
Additional Info:
STM32CubeIDE version: [your version, e.g. 1.13.0]
Toolchain: ARM-GCC (default from CubeIDE)
Request:
Could someone please help me identify why this "Permission denied" error is happening and how to resolve it? Also if the configuration has some other possible issue for ethernet not to work. I am attaching some conf images from cubeMX below





Thanks in advance!