Skip to main content
Associate
October 23, 2024
Question

STMCubeIDE v1.16.1 UI is Trimming Double Quotes when Adding Symbols to Project

  • October 23, 2024
  • 1 reply
  • 653 views

 Issue occurs in this build: 

davef_3-1729664793565.png

To reproduce: 

  • In an STM32MCU project right click properties
  • Navigate to C/C++ General -> Paths And Symbols
  • Select the Symbols Tab
  • Add a new Symbol and in the value field, reference an environment variable inside quotes e.g. "${PATH}" 
  • davef_0-1729664432067.png

     

  • Click save and the trailing double quote is removed
  • davef_1-1729664502095.png

 

The workaround is to edit the symbols elsewhere see below noting where I added the extra quote: 

davef_2-1729664689217.png

 

    1 reply

    STTwo-32
    Technical Moderator
    October 23, 2024

    Hello @davef and welcome to the ST Community.

    I'm sending this for internal investigation, and I will be back to you as soon as I have a clear answer.

    Best Regards.

    STTwo-32

    davefAuthor
    Associate
    October 23, 2024

    Thank you. Another thing I noticed is that system environment variables only seem to be refreshed on opening the workspace, is there a way to refresh the cached environment variables when running a pre compile action or script?