Strange behaviour when setting compiler variables - include paths - Bug report
Hello
I am using STM32CubeIDE
Version: 1.19.0
Build: 25607_20250703_0907 (UTC)
OS: Windows 10, v.10.0, x86_64 / win32
Java vendor: Eclipse Adoptium
Java runtime version: 21.0.3+9-LTS
Java version: 21.0.3
When I include libraries into my stm32 project I drag and drop a folder (from the windows explorer) int the project predefined folder "Drivers". In a second step I need to set the paths for the C-compiler, C++ compiler and linker seperately.
To do so I open the procect preferences and add a path for the C compiler: In this case The project name is TST_CCS811. and the folder to add is DebugPrintf. I click ok. - path for this folder set.

I continue to do so for the C++ compiler and the linker. The path is always the same - it works - paths set.

Now I want to add the next folder in this case GPIO_CPP.
To do so I click on the C compiler again but now - very strange - another project appears in this case TST_BME280 and not the TST_CCS811 which was selected before.

This is very annoying: If you do not recognize this strange behaviour you will add a wrong path (of another project) to jour compilers. It can take very long to find this error - trust me!
Regards
Alexander