Suppprt of LWIP package on NUCLEO-H563ZI from Discovery kit with STM32F769NI MCU
Hi,
When I worked on the Discovery kit with STM32F769NI MCU it supported in the STM32CubeIDE/MX the LWIP package (from 2025) with FreeRTOS/V1. Now when I pass my project to NUCLEO-H563ZI I see in the TM32CubeIDE/MX that ST will not support the LWIP with FreeRTOS anymore. FreeRTOS is only v2 in this board.
Is someone integrete the LWIP package on NUCLEO-H563ZI with FreeRTOS/v2? The code main files that should be changed from STM32F769NI to NUCLEO-H563ZI are LWIP/App/lwip.c, LWIP/Target/ethernetif.c/h, LWIP/Target/lwipopts.h, main.c.
Is there any project in git that have done this miggration for LWIP package (code from 2025) and using FreeRTOS/v2 in it's LWIP package? Or share with me those 4 LWIP files for NUCLEO-H563ZI board.
Thanks.