Skip to main content
Associate II
December 14, 2025
Question

The BLUENRG-M2SA is not responding,code enter goto end_label

  • December 14, 2025
  • 1 reply
  • 368 views

Hi,

I’m porting the DATALOG2 application from

fp-sns-datalog2\STM32CubeFunctionPack_DATALOG2_V3.1.0\Projects\STM32U585AI-STWIN.box\Applications\DATALOG2to the STM32U575VGT6, but I’m running into issues with the Bluetooth functionality during debugging. Does anyone have any suggestions? 

The code enters this section:

if (ret_status != (ble_status_t)BLE_STATUS_SUCCESS)

{

BLE_MANAGER_PRINTF("Error: HCI_LE_SET_SCAN_RESPONSE_DATA [%x]\r\n", ret_status);

goto end_label;

}

I can erase, read, and program the BLUENRG-M2SA using RF-Flasher Utility v4.5.0, which indicates that the chip is not damaged.

The complete project source code is attached.

The hardware circuit is as follows:

dzf_0-1765675626078.png

The code is as follows:

void set_connectable_ble(void)

{

#if (BLUE_CORE == BLUENRG_MS)

char local_name[8] = {AD_TYPE_COMPLETE_LOCAL_NAME,

#else /* (BLUE_CORE == BLUENRG_MS) */

uint8_t local_name[8] = {AD_TYPE_COMPLETE_LOCAL_NAME,

#endif /* (BLUE_CORE == BLUENRG_MS) */

ble_stack_value.board_name[0],

ble_stack_value.board_name[1],

ble_stack_value.board_name[2],

ble_stack_value.board_name[3],

ble_stack_value.board_name[4],

ble_stack_value.board_name[5],

ble_stack_value.board_name[6]

};

ble_status_t ret_status = BLE_STATUS_SUCCESS;

 

/* disable scan response */

#if (BLUE_CORE == BLUENRG_MS)

ret_status = HCI_LE_SET_SCAN_RESPONSE_DATA(0U, NULL);

#else /* (BLUE_CORE == BLUENRG_MS) */

ret_status = hci_le_set_scan_response_data(0U, NULL);

#endif /* (BLUE_CORE == BLUENRG_MS) */

if (ret_status != (ble_status_t)BLE_STATUS_SUCCESS)

{

BLE_MANAGER_PRINTF("Error: HCI_LE_SET_SCAN_RESPONSE_DATA [%x]\r\n", ret_status);

goto end_label;

}

 

/* Set the board discoverable */

if (ble_stack_value.advertising_filter == ((uint8_t)NO_WHITE_LIST_USE))

{

ret_status = aci_gap_set_discoverable(ADV_IND, ble_stack_value.adv_interval_min, ble_stack_value.adv_interval_max,

ble_stack_value.own_address_type,

ble_stack_value.advertising_filter,

(uint8_t)(sizeof(local_name)), local_name, 0, NULL, 0, 0);

if (ret_status != (ble_status_t)BLE_STATUS_SUCCESS)

{

BLE_MANAGER_PRINTF("Error: aci_gap_set_discoverable [%x] Filter=%x\r\n",

ret_status, ble_stack_value.advertising_filter);

goto end_label;

}

else

{

#if (BLE_DEBUG_LEVEL>1)

BLE_MANAGER_PRINTF("aci_gap_set_discoverable OK Filter=%x\r\n", ble_stack_value.advertising_filter);

#endif /* (BLE_DEBUG_LEVEL>1) */

}

}

else

{

/* Advertising filter is enabled: enter in undirected connectable mode

in order to use the advertising filter on bonded device */

#if (BLUE_CORE == BLUENRG_MS)

ret_status = aci_gap_set_undirected_connectable(ble_stack_value.own_address_type,

ble_stack_value.advertising_filter);

#else /* (BLUE_CORE == BLUENRG_MS) */

ret_status = aci_gap_set_undirected_connectable(0,

0,

ble_stack_value.own_address_type,

ble_stack_value.advertising_filter);

#endif /* (BLUE_CORE == BLUENRG_MS) */

if (ret_status != (ble_status_t)BLE_STATUS_SUCCESS)

{

BLE_MANAGER_PRINTF("Error: aci_gap_set_undirected_connectable [%x] Filter=%x\r\n", ret_status,

ble_stack_value.advertising_filter);

goto end_label;

}

else

{

#if (BLE_DEBUG_LEVEL>1)

BLE_MANAGER_PRINTF("aci_gap_set_undirected_connectable OK Filter=%x\r\n", ble_stack_value.advertising_filter);

#endif /* (BLE_DEBUG_LEVEL>1) */

}

}

 

update_adv_data();

 

end_label:

return;

}

#else /* ((BLUE_CORE != BLUENRG_LP) && (BLUE_CORE != STM32WB07_06) && (BLUE_CORE != STM32WB05N)) */

#if (BLUE_CORE == STM32WB05N)

 

 

 

 

 

1 reply

dzfAuthor
Associate II
December 14, 2025

my PCB layout is as following, does it led to the above question?

dzf_0-1765677250349.png