Lead
April 8, 2024
Solved
ThreadX thread and queue names not displayed properly in CubeIDE 1.15.0 debugger (STM32H5)
- April 8, 2024
- 11 replies
- 16804 views
New workspace
New STM32 project
Board Selector Nucleo-144 STM32H5 NUCLEO-H563ZI
Take the defaults
Set the tick to TIM6
Pinout & Configuration - Middleware and Software Packs - THREADX
Generate App Init Code - check
Save everything, compile, debug, put a breakpoint on the opening curly in tx_app_thread_entry (app_threadx.c).
Run and reach the breakpoint.
Window - Show View - ThreadX - ThreadX Thread List
Notice how the names are just the first character of the name strings.
This happens on queues as well. I suspect semaphores and mutexs will be the same.
This worked properly in a previous version of CubeIDE on STM32L4 if that matters.
Full cube project attached.